With these drives you can read and record DVDs and/or CDs in all kinds of different formats. Please notice the difference between DVD+R and DVD-R when buying a DVD burner, often drives can write only to one of those two media types, sometimes to both. When you buy a drive that only supports one type, you will always have to be careful to choose the right writable DVD discs at the shop. Newer DVD drives also support writing to Dual Layer DVDs. This kind of discs have a storage capacity of 8.5 GB instead of the usual 4.7 GB. DVD (re)writers generally can read and write CDs also, but only some CD (re)writers can read DVDs.
Release date: 22 Nov 2007
Info modified on: 09 Jun 2009 15:20:03
Product views: 0
This statistic is based on the
6815
using ecommerce sites (eshops, distributors, comparison sites, ecommerce ASPs, purchase systems, etc) downloading this ICEcat data-sheet since
22 Nov 2007.
Only sponsoring brands are included in the free Open ICEcat content distribution as used by
6324
free Open ICEcat users .
DVR-215DBK, High Speed Dual Format Drive with SATA Interface (Black)
With these drives you can read and record DVDs and/or CDs in all kinds of different formats. Please notice the difference between DVD+R and DVD-R when buying a DVD burner, often drives can write only to one of those two media types, sometimes to both. When you buy a drive that only supports one type, you will always have to be careful to choose the right writable DVD discs at the shop. Newer DVD drives also support writing to Dual Layer DVDs. This kind of discs have a storage capacity of 8.5 GB instead of the usual 4.7 GB. DVD (re)writers generally can read and write CDs also, but only some CD (re)writers can read DVDs.
- Max 20X writing speed for DVD-R/+R. - Max 10X writing speed for DVD-R DL / +R. - DL (Dual / Double Layer media). - Max 5X reading speed for DVD-RAM. - Multi-effect LCD Tilt Servo Compensator Mechanism. - Ultra-DRA (Dynamic Resonance Absorber) low vibration mechanism. - Performance adjusting firmware. - Disc-Resonance Stabiliser. - Supports "Buffer Under Run" protection (CD and DVD).
Specs
Alternatives
Options
Writing speed
CD write speed
40 x
CD rewrite speed
32 x
DVD+R write speed
20 x
DVD-R write speed
20 x
DVD-R Double Layer write speed
10 x
DVD+R Double Layer write speed
10 x
CD-RW write speed
4 x
Reading speed
CD read speed
40 x
DVD+R read speed
16 x
DVD-R read speed
20 x
DVD-R Dual Layer read speed
10 x
DVD+RW read speed
13 x
DVD-RW read speed
13 x
CD-R read speed
40 x
CD-RW read speed
32 x
DVD-RAM read speed
5 x
DVD-ROM read speed
16 x
CD-ROM read speed
40 x
Access time
DVD drive average random access time
130 ms
Access time
CD-ROM drive average random access time
120 ms
Optical drive
Internal
The device is built in, or needs to be built in (Yes/No). No, means that the device is connected externally via wire or wireless.
Loading mechanism
List of mechanisms by which the recording media is loaded into the product
Tray
Drive device, buffer size
2 MB
Interface
Interface ports to connect pieces of equipment. USB (Universal Serial Bus) has become the most popular wired interface to connect peripherals. USB 2.0 supports speeds up to 480 Mbit/s (USB 1: 12 Mbit/s). The interface FireWire is also known as the IEEE 1394 standard. Enhanced IDE (EIDE)is sometimes referred to as Fast ATA, Fast IDE or ATA-2.
Serial ATA
Mounting
Vertical/Horizontal
Record modes
Disc-at-once (DAO)
Session-at-once (SAO)
Track-at-once (TAO)
Multi session
Weight & dimensions
Dimensions W x D x H
Dimensions of the produkt (Width x Depth x Height) in millimeter.
148 x 180 x 42.3 mm
Weight
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.
800 g
Energy management
Power consumption
Amount of power consumed by this model; expressed in watts. Typical values that manufacturers give are power consumption when off, standby/suspended mode, typical use, maximum usage.